Home

Branch Locator

Area Links


HOME > Markets > Utility > Suppliers > Polywater

Polywater



In 1973, Nelson Jonnes, a Minnesota research chemist with more than a dozen patents under his belt, threw together some slippery ingredients in his basement and began selling it as a SCUBA diving-suit lubricant. It was well received, but the potential income from that alone could not support his family of six.

With a quick change of marketing focus in 1974, the fledgling company began selling the same technology to the telcom and power utility markets in the form of a unique, water-based cable pulling lubricant. It revolutionized the industry, which until then had used mud, wax, and grease. Polywater® Cable Pulling Lubricants have been the leaders ever since.

Today Polywater® manufactures products for high voltage splice preparation, hot-stick cleaners and wax, utility boom truck cleaners and wax, adhesives for HDPE conduits, sealants for leaking oil and SF6 gas transformers, foam duct sealants for conduits, rubber goods cleaner and fiberglass basement patch kits.

BonDuit® HDPE Conduit Adhesive

BonDuit® Adhesive creates airtight and watertight splices when joining HDPE  to PVC, rigid steel and fiberglass sweeps or conduits. Bonds are durable with high tensile strength within an hour. The strong bonds withstand movement and vibration. Great for transitioning HDPE pipe to a home, pole or transformer.

SpliceMaster® High Voltage Cleaner/Degreasers

"SpliceMaster® cleaners are available to meet different needs in cable and general electrical cleaning.  The SpliceMaster® PEL-PAC® package controls release and exposure to solvent vapors.  They share the following features:  Safer, controlled use.  No residue.  Meets IEEE 1493 requirements.  Excellent cleaners for electrical grime like shield picks, corrosion inhibitor, and silicone grease."


For more information on Polywater products, please visit their website at http://www.polywater.com