Wi-Fi vs. Cellular
Wi-Fi and cellular coverage are often talked about as though they are interchangeable – or a substitute for one another. However, it’s more beneficial for enterprises to consider the advantages of each and make room for both. Every enterprise has Wi-Fi – it’s great for stationary use – computers, printers / copiers, employees calling from an office, etc. But there are some specific advantages of cellular coverage – which is why both have their place as part of a comprehensive strategy.
As compared to Wi-Fi, cellular coverage:
- Is more secure
- Is more reliable with fewer interruptions
- Has less chance of traffic interference as it uses capacity from the macro network
- Requires no log-in for visitors, vendors, etc., and no one will lose coverage or have to re-login as they move throughout a large facility
- Offers access all major networks during an emergency
- Puts lets pressure on internal IT resources