With 20 years of industry leading technology, MaxCell® is one of the fastest growing brands in the network construction industry. Accepted by the Rural Utilities Service (RUS) and installed by the largest global telecom companies and cable Management Service Organizations (MSOs), MaxCell is the standard for maximizing conduit space while reducing total system costs.
The only flexible fabric innerduct solutions designed specifically for the network construction industry, MaxCell products conform to the shape of cables placed within, greatly reducing the wasted space associated with rigid innerduct options. Network owners and builders use MaxCell to increase cable density by as much as 300%. Faced with the challenge of deploying new infrastructure while minimizing costs, using MaxCell products reduces the number of conduits required for new network construction, minimizes the need for additional conduit in overlay applications, and enables incremental deployment to match system requirements.